This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTDX_Log_Event support in Debug Server Scripting?

I'm using Code Composer @ 4.2.4.00033.

I have an old VB application using a COM client with RTDX that i need to reproduce the functionality of for the newer code Composer. I've looked at the Debug Server Scripting examples and the loadti samples . I am not up to speed with java and/or javascript so i'm not sure if i just did not realize what i was seeing , but did not see specifically any references to RTDX_Log_Event or RTDX_Log_Event_Data. Is there an example of the host handling RTDX_Log_Events posted from the target ( in java or javascript ). Any help would be appreciated.

Thank You