Hi there,
Im using CCS v5.3.0.00090 on windows 8. I only recently reinstalled after a previous install was found to be corrupted.
Initilly everything seemed to be running fine but over the last few days the workspace error log keeps reporting some unknown error. It usually occurs some time after I build or save, though not always.
I have attached the exported error log that shows the two errors that occur. As can be seen it is mostly a eclipse core unknown error, but there is the very occasional (only once in this dump) set of invalid key binding errors (Ln 177 -202)
I appreciate that CCS is still unsupported on win 8, but thought this may be a known error or at the very least help with any efforts to make it supported...
Ta