Other Parts Discussed in Thread: CCSTUDIO
Hello,
When I try to build the PRIME example of the TMDSPLCKIT-V3 PLC kit I receive the following errors:
This is the log file content:
!SESSION 2013-04-01 15:39:44.265 -----------------------------------------------
eclipse.buildId=4.2.4.00033
java.version=1.5.0_14
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=ro_RO
Command-line arguments: -os win32 -ws win32 -arch x86
!ENTRY org.eclipse.update.configurator 2013-04-01 15:39:44.937
!MESSAGE Duplicate feature found on site platform:/base/ : com.sd.ccstudio.emulation
!ENTRY org.eclipse.update.configurator 2013-04-01 15:39:44.937
!MESSAGE Duplicate feature found on site platform:/base/ : com.ti.ccstudio.product
!ENTRY org.eclipse.update.configurator 2013-04-01 15:39:44.937
!MESSAGE Duplicate feature found on site platform:/base/ : com.ti.cgt.c2000.6.0
Console message:
gmake: *** [c:/temp/f2806x/phy_tx_rx/Debug/F2806x_CodeStartBranch.obj] Error 1
gmake: *** [c:/temp/f2806x/phy_tx_rx/Debug/F2806x_GlobalVariableDefs.obj] Error 1
gmake: *** [c:/temp/f2806x/phy_tx_rx/Debug/F28335_init.obj] Error 1
gmake: *** [c:/temp/f2806x/phy_tx_rx/Debug/test_tx_rx.obj] Error 1
gmake: Target `all' not remade because of errors.
I am using the CCS 4.2.4. which is compatible with my kit, on another computer I don't receive this errors. How can I make this errors disappear I don't understand where the duplicate is. Are this errors important or I can ignore them ?