My project is using CCS 5.3 to generate code for the DSP on the DA830/L-137. I use IPC v1.0.5.60, SysBios 6.21.0.13 and XDIAS 6.25.1.08. My compiler is 6.1.13.
Occasionally something happening in the DSP causes CCS to start ringing the bell in my PC. That is, it triggers the bell sound. I've heard it both with CCS4 and CCS5. It's got to be trying to tell me something. What can it be? My code is writing to the RTA logs. Is it possible for something there to ring the bell?