This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD XDS560v2 STM getting slow when using RTDX

Hi,

I'm using a SD XDS560v2 STM Emulator with a custom C6415 hardware. If I enable RTDX within the BIOS config file, operations like loading programs or resetting the CPU get very slow. This only happens if I use the USB connection, the ethernet connection works fine.

Components used:

  • CCS V 5.3.0
  • Spectrum Digital Emulators 5.2.0.07
  • DSP/BIOS: 5.42.0.07

Thanks,
Ralf

  • Hi Ralf,

    I see this also. I filed a bug for this. The tracking ID is: SDSCM00046908

    Note that RTDX is not supported anymore. We will completely phase it out by CCSv6. So a timely resolution of this issue is unlikely. Sorry.

    Thanks

    ki