This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using CCSv5.2 along with XDS100v2 for debugging Pandaboard. I have created a CCS project and have been trying to perform read/write operation on Keyboard registers but CCS is not able to read registers. It gives an error of unable to read.
However i am able to read/write Pad control and core registers.
I am attaching snapshots of the same. Please suggest solution for this problem.
Aniket
Aniket,
I was not successful in accessing the keyboard controller registers on my Pandaboard as well. However, that does not mean a bug.
Several peripherals do not allow their registers to be accessed unless they are powered up. Also, some peripherals also require system registers properly configured to allow access to these.
Unfortunately I am not an expert on the OMAP4 device to have an example code that enables the keyboard controller - for that you will have to check the suggestions from the experts on the device forum.
Regards,
Rafael
Hi,
Your are right.. After configuring proper system registers i am now successfully able to access keyboard registers.
Thank you.
Aniket