This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All,
I am a new user in DSP programs.
I prepare the experimenter kit of TMS320F28335.
I have installed the CCS5. and set the connection to XD100 V3.
When I press the "Test connection" button, I face to error!
How can I solve the problem?
With best regards,
Ras,
I am not sure but you might have to select XDS100v2 instead.
Regards,
Maciej
Ras,
Are you sure it is an XDS100v3 that you have? Those are pretty rare as they are really just for devices that use cJTAG instead of JTAG which is not the case for F28335.
Most of the experimenter kits had on onboard XDS100v1 or XDS100v2. For a lot of them it is the older XDS100v1.
This doc has some more information on how to connect:
http://www.ti.com/lit/ml/sprufr5f/sprufr5f.pdf
Regards,
John
Dear All,
One can solve the problem by following the bellow link
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/21086.aspx
Regards,
Ras