This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using CCSv5.x with DSP/BIOS 5.20.x



Hello,

Is it possible to use CCSv5.x (hopefully, CCSv5.3) with DSP/BIOS 5.20.x ?
I'm asking this because I'm wondering if CCSv3.x may be mandatory whenever we need DSP/BIOS from ROM at C672x devices.

The following document says DSP/BIOS v5.20.x and CCSv3.x can be used when using romized DSP/BIOS, but CCSv3.x is too old to use for me.

http://www.ti.com/lit/an/spraas8/spraas8.pdf

The almost same discussion was posted at the following link, but no validated answer for the query. 

http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/228216.aspx

Best Regards,
Kawada