Hello,
referring to
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/234467.aspx
I used the same subject as in the thread above.
I have to mention, that I really downloaded twice the install software of CCSv5 and both times it did not work on a machine with W7/32Bit prof.
Between each installation I also deleted the Jammer-directory and the Ti-directory as well.
I don't have any anti vrus active while installing CCS.
I personally cannot do anything with the attached Logfile:
2656.ccs_setup_5.3.0.00090_install.zip
Hope there is any help in this cas. Thank you.
Dieter