This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

hex6x utility error

hello everyone 

i am working on dsk6713

when i tried to make a hex file using hex6x utility i got erro which is shown in  attached file.....

my linker command file for hex6x utility....

flash_sine.out
-a
-image
-zero
-memwidth 16
ROMS
{
PMEM: org=0x00000000, len=0xFFFF, romwidth=16
FLASH: org=0x90000000,len=0x00080000 files={flash_sine7.hex}

}
SECTIONS
{
.vecs: paddr=0x00004600
.text: paddr=0x90000030

.const: paddr=0x00004000
.cint: paddr=0x00005050
}

 

what are the additional files required for flash burn ? 

i have also made .lsb and .msb files of .out file...

i have followed the procedure written in help of ccs studio for hexconversion utility......

is there anything that needs to be specified in linker command file?

how to define boot load in sections? and it will start from which memory location ?

regards

jay sompura

7220.Doc1.docx