Other Parts Discussed in Thread: MSP430FR5739
Hi,
I have been having some issues for a few weeks now with CC5.3 failing to compile my files as it cannot find them.
I have just had a case tonight where I made some edits to my code, which compiled fine, I changed the include directory order in the settings and after that the code could not be located.
To resolve this I currently check in all my code, check it out in a new project and start again (I am using the SVN client plugin)
I had been working with CC4.x.x the exact versions I am not sure, but after the upgrade to 5.xx these issues have appeared.
I dont really want to delete my workspace as I have various example project etc that I have built up, though some of these do exibit the same "cannot find files issue".
I have seen a few other posts on this issue, none of which seem to help me, and I am just wondering if anyone else out there is experiencing something similar and what can be done to resolve it.
I should also state that it seems mostly to manifest itself on code composer restarts.
I do apologise that this is somewhat vague, as I find more info ill post