This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccsv5_full_symb_debug.



Hi:

We are using  CCS Version: 5.1.0.09000. Our platform is based on the OMAP L138 (240 MHz). We have ported our code from the OMAP 5912 to the L138. The old platform was running under CCSv3.1. Now on the new platform when I run the code under CCSv5 with 'full symbolic debug' enabled, I am running out of MIPS and I am unable to debug. How do I get around this problem without increasing the OMAP clock? Could you please help?

Thanks a lot!

Cheers,

Mushtaq

  • hello Mushtaq,

    Mushtaq Syed said:
    when I run the code under CCSv5 with 'full symbolic debug' enabled, I am running out of MIPS and I am unable to debug.

    I'm not sure how running with full symbolic debug is causing your application to run out of MIPS and unable to debug. Could you please explain this?

    ki

  • Hi Ki-Soo:

    When I enable 'Full Symbolic Debug' and build the DSP code, the size of the DSP code goes up to 6863723 (see below). If I use this, then I get underruns (see ALSA lib pcm.c:7339:(snd_pcm_recover) underrun occurred below); however, if I strip off the debug code using the TI utility strip6x, then I don't have this issue.

    Thanks a lot!

    Cheers,

    Mushtaq


    -rw-------    1 root     root       6863723 Apr 19 10:16 audion.out
    -r--------    1 root     root        268021 Apr 18 09:40 audion_orig.out


           0.691 DSP: Version Minor: 8
           0.691 DSP: Product Minor Version: 0
           0.692 DSP: Product Revision: 0

           0.692 DSP: SE VERSION HIGH BYTE: 28

           0.692 DSP: SE VERSION LOW BYTE: 15

           0.723 Ignoring: CodReadCnt = 1, nBytesRead = 1152
    ALSA lib pcm.c:7339:(snd_pcm_recover) underrun occurred
    ALSA lib pcm.c:7339:(snd_pcm_recover) underrun occurred
          11.675 [at.c]: ProcessResult AEC Configuration Test Results  ERL1: -6.9 dB ERL2: -6.9 dB ERL3: -6.9 dB ERL4: -6.9 dB
          11.676 [at.c]: ProcessResult AEC Configuration Test Results  ERLE1: 0.0 dB ERLE2: 0.0 dB ERLE3: 0.0 dB ERLE4: 0.0 dB
          11.677 Posting q.semTerminate1...
          11.679
          11.680 TRM: Current date and time: Fri Apr 19 10:18:18 2013
          11.681 TRM: B0:E54:? Normal Termination
          11.683

    /g3n/badge/data/log.txt written.
    [root@badge bin]#

  • Mushtaq Syed said:
    When I enable 'Full Symbolic Debug' and build the DSP code, the size of the DSP code goes up to 6863723 (see below)

    Yes, the out file size gets bigger because there is more symbolic information in the out file. This is fully expected. Note that this size is NOT your actual target code size. The symbols get loaded into the debugger, not the target. The actual target code is just a part of the out file.

    Mushtaq Syed said:
    If I use this, then I get underruns (see ALSA lib pcm.c:7339:(snd_pcm_recover) underrun occurred below); however, if I strip off the debug code using the TI utility strip6x, then I don't have this issue.

    All the strip does is remove the debug symbols. Your actual DSP code is the same. So really your target application should not run any different.

    I don't know what this "underrun" is. Is that message coming from the target application?

  • Hi Ki-Soo:

    Yes, the message is coming from the target application. As, I had mentioned in my first post, our platform has an OMAP L138 running under Linux. The underruns are from the ALSA audio codec driver. These underruns do not occur when I strip off the debug information.

    Thanks a lot!

    Cheers,

    Mushatq

  • Hi Ki-Soo:

    Yes, the underrun message is coming from our target application. As I had mentioned in my first post, out platform is based on the OMAP L138 running under Linux. The underrun messasges are from the ALSA audio codec driver. Underruns do not occur if I strip off the debug information.

    Thanks a lot!

    Cheers,

    Mushtaq

  • Can someone please point me where I can find the strip6x application?  I am using CCSv5 with the C2000 family.

    Thank you!

  • Cyril Lance said:
    Can someone please point me where I can find the strip6x application?  I am using CCSv5 with the C2000 family.

    You'd want to use strip2000 instead. It comes with your compiler install:

    <CCS INSTALL DIR>\ccsv5\tools\compiler\c2000_<version>\bin