I have an issue with Uniflash 2.1.0 on just one PC, running Windows 7 64-bits. We work with two types of targets, MSP430 and TMS320C2000. For MSP430, the CCS Uniflash software is able to recognize the MSP-FET430UIF tool, and I can burn the images onto the targets just fine. However, for a TMS320F28335 target, I get the following:
[13:30:32] Begin Launching session operation...
[13:30:32] ERROR >> Unable to load ..\..\..\emulation\tpi\tpi28xx.dll: The referenced assembly is not installed on your system.
[13:30:33] ObjectEventCallback error!!! com.ti.debug.engine.IApplication$InitializationException: Unable to load ..\..\..\emulation\tpi\tpi28xx.dll: The referenced assembly is not installed on your system.
[13:30:33] Operation Launching session returned.
This both for Spectrum Digital's XDS100V2 and XDS510USB emulators. Drivers are installed properly for both.
I've tried a complete uninstall and reinstall for Uniflash, as well as the previous version (V1), but nothing worked. On other PCs with same configuration in the lab, I can burn both MSP430 and TMS320C2000 targets without any problem. We have standard images on the PCs, so the possibility of the PCs having different versions of operating system is highly unlikely. Maybe it is an installation issue, but I've not been able to figure out what is the right way of installing Uniflash. Also, I'm installing it the same way on other PCs, so can't think of what could be the difference here.
Thanks
-Ahmad