This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to import the GUI for HVPSFB kit to GUI Composer for modifications?

Hi Everybody,

I would like to modify the existing HVPSFB kits' VMC GUI for my own use. But somehow I couldn't import it to the GUI composer. In Control Suite there are Source and Application files. Is there any way to open the corresponding file extension in GUI composer environment?

Thanks

  • Actually was the kit's GUI created with GUI composer or in C# ?

  • Hi Ekrem, 

    I don't think that particular application is using GUI Composer. I took a quick peek and it looks like it is just a .NET application, thus you would probably need to use MS Visual Studio to open it. I think recent Motor Control kits leverage GUI Composer, but not all GUIs that are part of Control Suite. You may also want to post in C2000 forum to see if there is more information on which GUIs can be developed further and which tools to use.

    Martin