Other Parts Discussed in Thread: TMS320F28335
1. Build the program, there is no error or warnning
2. Link was success, and no error or warnning
3. choice the project, choice the "Debug As" option
4. the CCS5 give me infomation as following:
C28xx: Breakpoint Manager: Retrying with a AET breakpoint
C28xx: Trouble Setting Breakpoint with the Action "Process CIO" at 0x62e00: (Error -1066 @
0x62E00) Unable to set requested breakpoint in memory. Verify that the breakpoint address is
in writable memory. (Emulation package 5.0.872.0)
C28xx: Breakpoint Manager: Retrying with a AET breakpoint
C28xx: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x65195: (Error -1066
@ 0x65195) Unable to set requested breakpoint in memory. Verify that the breakpoint address
is in writable memory. (Emulation package 5.0.872.0)
So the device and the CCS5 not running as normal, the debug action was fail.
So, I need you help to analyze and resolve those error and warnning, help to start debug programming.
Best Regards,
Roc