This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'd like to use intrinsics in my project, but an error occurs when I try to build it .
Here is a part of my source code:
#include <c6x.h>
void main (void)
{
/// some code
__x128_t r, a={1,1,1,1};
long long b=1;
r=_cmatmpy(b,a);
/// some code
return;
}
As I know, intrinsics are compiler's built in functions, I also included "c6x.h", but _cmatmpy is still unresolved symbol.
I use C6678 simulator and Code Generation Tool v. 7.4.2.
Thank you in advance.
Perhaps omp_matvec.obj is left over from a time when it was compiled without -mv6600. Please make the project clean and try again.
Unfortunately, it doesn't help...
One more thing... I've found out some DSPLIB's 3.1.1.1 functions (for example DSP_mat_mul_cplx) uses the same intrinsics. So, if I use that function (with the same intrinsics in theirs source code) there are no problems in project building.
I'm not sure, but could it be the way to find a reason of my problem?
It still seems like something basic is wrong. Please show exactly how this source file is built, along with the resulting diagnostic. You can copy-n-paste that from the CCS build console window.
Thanks and regards,
-George
Here are result diagnostics:
**** Build of configuration Debug for project Dpl_080413_mtx ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: ../omp_config.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_23_04_60/xs" --xdcpath="C:/ti/omp_1_01_03_02/packages;C:/ti/bios_6_33_06_50/packages;C:/ti/ipc_1_24_03_32/packages;C:/ti/pdk_C6678_1_1_2_5/packages;C:/ti/uia_1_02_01_08_eng/packages;C:/ti/ccsv5/ccs_base;C:/ti/dsplib_c66x_3_1_1_1/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.omp.examples.platforms.evm6678 -r debug -c "C:/ti" "../omp_config.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring omp_config.xe66 from package/cfg/omp_config_pe66.cfg ...
cle66 package/cfg/omp_config_pe66.c ...
'Finished building: ../omp_config.cfg'
' '
'Building file: ../omp_matvec.c'
'Invoking: C6000 Compiler'
"C:/ti/bin/cl6x" -mv6600 --abi=eabi -O3 --symdebug:skeletal --optimize_with_debug=on --include_path="C:/ti/include" --display_error_number --diag_warning=225 --diag_wrap=off --gen_func_subsections=on --debug_software_pipeline --openmp --opt_for_speed=5 --gen_opt_info=2 --call_assumptions=2 --auto_inline=3 --preproc_with_compile --preproc_dependency="omp_matvec.pp" --cmd_file="./configPkg/compiler.opt" "../omp_matvec.c"
"../omp_matvec.c", line 57: warning #552-D: variable "r" was set but never used
'Finished building: ../omp_matvec.c'
' '
'Building target: Dpl_080413_mtx.out'
'Invoking: C6000 Linker'
"C:/ti/bin/cl6x" -mv6600 --abi=eabi -O3 --symdebug:skeletal --optimize_with_debug=on --display_error_number --diag_warning=225 --diag_wrap=off --gen_func_subsections=on --debug_software_pipeline --openmp --opt_for_speed=5 --gen_opt_info=2 --call_assumptions=2 --auto_inline=3 -z -m"Dpl_080413_mtx.map" -i"C:/ti/lib" -i"C:/ti/include" --reread_libs --warn_sections --rom_model -o "Dpl_080413_mtx.out" -l"./configPkg/linker.cmd" "./omp_matvec.obj" -l"C:\ti\dsplib_c66x_3_1_1_1\lib\dsplib.ae66" -l"C:\ti\dsplib_c66x_3_1_1_1\lib\dsplib.ae66e" -l"libc.a"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_cmatmpy ./omp_matvec.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Dpl_080413_mtx.out" not built
>> Compilation failure
gmake: *** [Dpl_080413_mtx.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Unfortunately, I am still unable to reproduce your results. Is there any chance you could send the entire CCS project?
Thanks and regards,
-George
Sure, here you are.
Please let me know if you need any information from workspace directory.
Regards, Maxim
I apologize for the delay.
Thank you for submitting the project. I can use it to reproduce the error. I filed SDSCM00047237 in the SDOWP system to have this addressed. Feel free to follow it with the SDOWP link below in my signature.
Thanks and regards,
-George
Thank you for your help, George.
I'll follow it and wait for the solution.
Regards, Maxim