This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Im using Code Generation Tools V5.2.12 (and I also tried V6.1.1).
Code generated is for a TMS320C28346 DSP, fpu32 float_support is enabled in compiler options.
When using the intrinsic "__f32toi16r" I get an internal compiler error as shown below:
===========================================================
'Building file: ../controller.c'
'Invoking: C2000 Compiler'
"C:/Programme/Texas Instruments/C2000 Code Generation Tools 5.2.12/bin/cl2000" --silicon_version=28 -O3 --define=LARGE_MODEL --include_path="C:/Software/CTR V4.20/Include" --include_path="C:/Programme/Texas Instruments/C2000 Code Generation Tools 5.2.12/include" --display_error_number --issue_remarks --large_memory_model --unified_memory --disable_dp_load_opt --float_support=fpu32 --rpt_threshold=64 -k --preproc_with_compile --preproc_dependency="controller.pp" "../controller.c"
>> ..\controller.h, line 168: INTERNAL ERROR: Illegal use of intrinsic: __f32toi16r
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!
>> Compilation failure
gmake: *** [controller.obj] Error 1
===========================================================
The Code where I'm using the intrinsic looks like:
inline int MultiplyAndRoundToInt(float a, float b)
{
float temp = a * b;
return __f32toi16r(temp);
}
Is this a compiler bug?
Best regards
Markus
Markus,
It looks like the internal error is coming from controller.h. Simply compiling those C source lines does not generate the error for me.
Could you attach a preprocessed version of controller.c so we have everything needed to reproduce the error?
This page describes how you can generate a preprocessed version of the source file:
http://processors.wiki.ti.com/index.php/Preprocess_Complex_Source_Code_for_Bug_Submissions
Just curious, does changing a,b and temp from float to double make the error go away?
Hi
Changeing the datatype from float to double makes not difference.
For convenience I have attached a very small Test-Project where the error occurrs.
Can you reproduce the error?
Markus
P.S. I'm out of office next week, so I cannot reply to any posts.
Thank you very much for the test case with which I was able to reproduce the internal error. As mentioned by Archaeologist he already submitted a bug report and the issue is being tracked in bug SDSCM00047070. You may track the status of the bug using the SDOWP link in my signature.
The fix will be in the C2000 6.1.4 release which is scheduled for May 28th.
-Mack
Hi
I have a rather big project where I would prefer to stay at Code Generatoon Tools V5.x.y (actual V5.2.12) instead of changeing to V6.x.y as this would result in a huge testing procedure. So, if it would be possible to include the fix in Code Generation Tools V5.2.13 I would be very happy :-)
Is this possible?
Markus
We do not have any plans to release the next 5.2.x release (5.2.16). The 5.2.15 was released less than a week ago. It does not contain the bug fix. If you need the fix, the best option would be to upgrade to 6.1.4 when it is released later this month.
-Mack