Hi,
I had trouble to debug code in previous CCS build (not sure but should be Version: 5.3.0.00030). The problem was not initializing the debug session. It was appearing a window that I need to upgrade the FET-430UIF. When I unplugged and plugged the USB cable it was sometimes works proper but not all tries. Then I upgraded the CCS hopping that will be ok.
But now, I am getting the “Error initializing emulator: Could not set device Vcc” error window.
I tested it with MSP-EXP430F5528 board with external battery. But it still gives the same error. After getting the error, I try to get the firmware version of the FET from Fet-pro430 software and got the firmware version “0…” But, when I unplug and plug the cable, I could get the expected FW version.
FET-430UIF hardware is V1.4a and FW version is 3.02.05.004
Any help will be appreciated. Thanks.