This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
msg m26_t[25];
int get_fastCorrection (Sat* Sat, msg * msg1, msg[4][2], msg24_t[15], msg * msg6, msg * msg10, msg * msg7, double eps_ltc_m, int rnd_options[8]);
I have multiple arrays in my code like this and the error is the same every where "which is array is too large" and I am using code composer studio 5.3.0
could any one please try to help me
Thank you.
Where is this error message coming from? The linker?
ravi raj1 said:I have multiple arrays in my code like this and the error is the same every where "which is array is too large" and I am using code composer studio 5.3.0
It may be coming from the compiler. Which target processor are you working with (MSP430, C2000, C64x+ etc..) and what sized arrays are these errors coming for? Could you provide a sample of the code where these errors are generated? If you look at the CCS build console instead of the Problems view and if it shows the line numbers where the error is coming from that should help identify the arrays that it is complaining about.
I have both the views on my screen sir the console and the problems and yes i know the errors where they are coming from also because of the line number mentioned ,here are my arrays where i am getting array too large errors sir
msg m18_t[11],
msg msg24_t[25],
msg msg25_t[15],
msg m26_t[25],
char m18_char[5][263],