This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compilation Problem with Runtime function " system"

Hello,

The following c code isnot compiling in CCS version 5.3 or 5.1

The processor is : C6748.

#include <stdlib.h>

int main(void)
{

    system("move /Y C:/Source/SineWaveFromADC.txt C:/Destination\n");

    return 0;
}

This is the message error plot in CCS console:

**** Build of configuration Debug for project RunTimeFunction_CCS53 ****

"C:\\ti\\CCSV5.3.0\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: C6000 Compiler'
"C:/ti/CCSV5.3.0/ccsv5/tools/compiler/c6000_7.4.1/bin/cl6x" -mv6740 --abi=coffabi -g --include_path="C:/ti/CCSV5.3.0/ccsv5/tools/compiler/c6000_7.4.1/include" --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"
'Finished building: ../main.c'
' '
'Building target: RunTimeFunction_CCS53.out'
'Invoking: C6000 Linker'
"C:/ti/CCSV5.3.0/ccsv5/tools/compiler/c6000_7.4.1/bin/cl6x" -mv6740 --abi=coffabi -g --display_error_number --diag_warning=225 --diag_wrap=off -z -m"RunTimeFunction_CCS53.map" -i"C:/ti/CCSV5.3.0/ccsv5/tools/compiler/c6000_7.4.1/lib" -i"C:/ti/CCSV5.3.0/ccsv5/tools/compiler/c6000_7.4.1/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --rom_model -o "RunTimeFunction_CCS53.out"  "./main.obj" -l"libc.a" "../main.cmd"
<Linking>

 undefined first referenced
  symbol       in file     
 --------- ----------------
 _system   ./main.obj      

error #10234-D: unresolved symbols remain

Question:

Do you know while the linker didn't getreach the code corresponding to the function "system"?

How can i solve this "unresolved symbols" problem?

Thanks