This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to re flash a GUI image into Piccolo F28035 controller using Controlsuite.



Could anyone please explain the procedures in re flashing a GUI image into Piccolo F28035 controller using CCSv4 or CCSv5.

when I tried to re flash and work with the GUI  there appeared error as given below:

  • There was no error message or screenshot attached. Could you please let us know the error you are seeing?

    To reflash an executable (.out) using CCSv5, you can launch a debug configuration (see  the "Launching a project target configuration manually" and "Launching a shared target configuration manually" videos in this page and use the one that applies to your case). Then you can simply load the executable using menu Run->Load->Load Program or Reload Program if you just reloading a program that was previously loaded.