When I step through code in CCS5.3, my expressions are not updating properly while debuggin, as shown on the bottom. Below is the summary of combinations that I tried. The question is, can my FETUIF be faulty?
MSP-FET430UIF CCS5.3 on Windows 7 - Debugger does not update
MSP-FET430UIF CCS5.3 on Linux Ubuntu 12.03 - Debugger does not update
MSP-FET430UIF IAR Workbench Windows 7 - Debeger does update
MSP-EXP430FR5739 Launchpad - CCS5.3 and Windows 7 - Debugger does update
My FET has white label on the back "V1.4a" and another label says "10086552009R", so what the heck is going on? Are there other revisions of MSPUIF?
Below is more detailed description of what is going on. All four scenarios above were done the same way.
The g_time_msec is initialzed and set to zero on line 17, but when main is entered g_time_msec is at 9. Why?
when line 22 is executed, g_time_msec changes to zero.
When line 25 gets executed, g_time_msec goes back to 9 Why? there is no interrupts on the background that would do that.
As I step through program the g_time_msec stays at 9.
Int ital post is located here:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/262643.aspx