This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

nm6x output

We use nm6x (v 7.3.1) to generate sym file for our in house debugging facility, on C6657 based system.

Some of the debug functions, such as test_dsp_logger comes with size of 0 ([36374] |0x81037258|    0|GLOB |FUNC |HIDN |89    |test_dsp_logger), while the function (regular, not static or inline) has proper code within it. I am attaching both the out file as well as the output of nm6x

The nm6x is called as following.

nm6x -g -l -o platform.nm platform.out

Is there any other options I should use?

thanks

Weichun

0535.platform.zip