Hi,
My development platform is Ubuntu 12.04 and my target is noted in the subject. I currently using CCS 5.2, but apparently the C/C++ compuler it uses (4.9.5) does appear to support hardware floating point, e.g. __sqrt(). As a consequence, I need to resolve this issue as soon as possible. I've made several attempts upgrading my copy of CCS but they fail (i.e. no choices provided or no upgrade indicated).
I want to try a different tact, what is the latest TI C/C++ cross compiler available for Linux, and if it's tied to CCS, what is the latest release of CCS available?
I would appreciate a link to any of the upgrade you may suggest, if any. Also, if there are no upgrade can you offer any suggestions to deal with my issue? Thanks
In the meantime, I've had to consider alternative compiler options for my TI LM4F target, like GNU. I have the GNU cross compiler running but at first glance it doesn't appear it's generating hardware floating point instructions either so I need to get support on the right forum. Where would I go to get this kind of help--which would be specific to the TI target?
Thanks in advance for your help.