This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSK6713 USB communication problem in I-5 processor



dear all,

                  Till date i have used dsk6713 with my dual core and I-3 processors but now i have updated my system to I-5 processor. When i tried to connect DSK6713 to system powered by I-5 processor am not able to connect the board. The usb enumeration which usually happens when connecting the 6713 is going into continues loop.

I have tried to work with ccs3.1 and also tried with ccs4.2 still am not able to connect the board.

please somebody provide the necessary solution in order connect the 6713 with I-5 system.

  • Mallesh,

    Since this is a CCS question and not a device question, it belongs in the Code Composer Forum instead of this C67x Single Core DSP Forum. A moderator will be asked to move this thread there, this time.

    Which Windows OS were you using with the I-3 and which Windows OS are you using with the I-5?

    Have you tried CCSv5 which is the latest release? CCSv4 is now quite old.

    Regards,
    RandyP

  • Mallesh,

    RandyP said:
    Which Windows OS were you using with the I-3 and which Windows OS are you using with the I-5?

    Please also specify if the OS on both machines are 32 or 64-bit

    Thanks

    ki