Other Parts Discussed in Thread: OMAP-L137
Hi Ti.
Is there a limitation that prevent me from using the OMAP-l137EVM onboard Jtag onboard Emulator, running a free or 90 days CCS5.4 license?
In the Target Configuration:
If I select the onboard "Spectrum Digital DSK-EVM PLUS onboard USB Emulator" there is only one board type available, the EVMDMR45X, trying to make the "board" myself by selecting a ARM9 and the C674X from the CPU library and add the .gel file from ccsv5\ccs_base\emulation\boards\evmomapl137\gel\evmomapl137_dsp.gel or browsing for a board all ends blind.T
The test under target configuration says :
[Start]
Execute the command:
%ccs_base%/emulation/drivers/sdjtag.exe -f %boarddatafile% -v -X reset -X scantest
[Result]
** BoardFilePath: C:\Users\CLAUSR~1\AppData\Local\.TI\693494126\0\0\BrdDat\testBoard.dat
** Resetting Emulator
-- Emulator is Reset
** Emulator Scan Test
-- Found JTAG IR Length of 6
-- Found 1 device(s) in the scan chain
[End]
Have also tried with a 90 days license with the same problems.
Have also tried on two machines, one win7 and one XP.
Have tried to build Target configuration using "Spectrum Digital SDS510USB with same results.
It looks like some thing is missing in the library, one installation had all option selected in the installation the last only what I expected to need. Same experience!!
CCs5.3 or 5.4 make no difference.
The target board is a OMAP-L137EVM from Spectrum digital rev "I".
Claus.