Hi,
I currently have CCS v5.2.1 with which I want to use a Blackhawk USB560v2 debugger. Fom the release notes I can see I need to update CCS v5.2.1 with Blackhawk Emulation Drivers v5.2.0.203. However because of company firewall issues, it's not possible for me to update directly from the CCS Update Manager. Do you have a zip file for all the necessary Blackhawk drivers which I can point the Update manager to? This will allow me to install the patch locally
Thanks, Taz