This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c code in code composer studio



Hello sir/madam,

How can i use c code in code composer studio?.

it is giving error, when i use the simple c coding., even i am not able to get the input by using "scanf".

I am using c6000 family of varient generic devices,c62xx.

I got some default warnings like :

WARNING 1:#10210-D creating ".stack" section with default size of 0x400; use the -stack option to change the default size add    C/C++ Problem

WARNING 2: #10210-D creating ".sysmem" section with default size of 0x400; use the -heap option to change the default size add    C/C++ Problem

When i use scanf, i can built the code and debug, but i couldn't run.

Also, please help me in code which can be applicable for code composer studio.