Other Parts Discussed in Thread: CCSTUDIO
Hi everybody,
I am trying to start a project using the Spectrum Digital ezDSP F28335 Kit. I'd like to remark that this kit uses an on-board emulator to connect the PC and the board, and it is not necessary to use a physical JTAG. The board is properly detected, I can run properly the CCSv5 and launch the debug session, but every time that I try to connect the board, the system shows a message like this:
Error connecting to the target:
Error 0x80002280/-1250
Fatal Error during: Target Communication, OCS, Control,
Device driver: Lost USB connection to emulator.
You should ABORT and restart to re-establish the USB link.
I have tried all the options that I found: reinstall the CCS and the drivers of the board, try in another computer to see if the problem is the PC,... But I have the same result with all the test that I made. Can someone help me with my problem?
Thanks in advance,. Regards,
Javier