Dear all,
I installed CCS 5.1 in my pc and i am trying to find the examples, how can i get examples and can anyone explain the after creating file, what the things to be add to file before debugging
Thanks
Kishore
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
I installed CCS 5.1 in my pc and i am trying to find the examples, how can i get examples and can anyone explain the after creating file, what the things to be add to file before debugging
Thanks
Kishore
Hi Kishore,
my recommendation(s) and tips:
1 - my very strong recommendation is to first install the current version (v5.4) with a full new installation into a simple directory like c:/myccs. You will find many improveements including to the Help : )
2 - Inside CCS the actual help is under Help->Help Contents
3 - Examples are found in the resource explorer Help->Welcome to CCS OR in the new project wizard (limited examples)
4 - See our great wiki (I have posted the main page and the training page here for you)
http://processors.wiki.ti.com/index.php/Code_Composer_Studio_V5
http://processors.wiki.ti.com/index.php/Category:CCS_Training
5 - normally you don't need to "add" anything ... simply press debug. However depending on the hardware you intend to use you may need to add in a library or you may need to create a target configuration file for your project (file ->new->target configuration file). However I would start with the examples and workshops as these will get you into these topics as well.
I hope this helps!
Best Regards,
LIsa
Dear lisa,
Thanks for your comments and nice documentation and i feel it would be better to provide me basic example files like blinking led project (which is basic in V3.3), i tried to search in v5 ((as when i am choosing the C2000/ TMS320F2835, in examples its not showing)).
Thanks
Kishore
another question ..I tried to build a small program of Helloworld and i got the following errors ..can you please tell where i am doing error pls
(1)
Description Resource Path Location Type
#10099-D program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x18f2 page 0. Available memory ranges: RAML1 size: 0x1000 unused: 0x1000 max hole: 0x1000 28335_RAM_lnk.cmd /hh line 125 C/C++ Problem
(2)
Description Resource Path Location Type
errors encountered during linking; "hh.out" not built hh C/C++ Problem
Hi Kishore,
a few comments
- I would recommend you go the training link I sent you and start with some of the workshops. There is even one that uses a c2000 part
- the error you recieved basically means the code is too large for the device. This may be the case or else better memory assignment migth be required
- if you don't need/use BIOS ... the easiest way to migrate is to import your old projects ... Project->Import legacy ccsv3.3 project
Also again ... I would strongly suggest a full fresh installation of the latest version fully unzipping and installing to a local simple folder.
Best Regards,
Lisa