Other Parts Discussed in Thread: TMS320F28035
Hi,
I'm working on a TMS320F28035 device.
I would like to have some of the code in RAM.
I'm doing it by adding the following to the linker command file:
ramFunctions : > progRAM, PAGE = 0
{
rts2800_ml.lib(.text)
DSP2803x_CpuTimers.obj(.text)
C28x_InstaSPIN_BLDC_Lib.lib(.text)
DLOG4CHC.obj(.text)
}
Where progRam is located in the RAM.
All works fine, except that I get an error at the "rts2800_ml.lib(.text)" statement. It says "file not found"
For all other files (DSP2803x_CpuTimers.obj, C28x_InstaSPIN_BLDC_Lib.lib and DLOG4CHC.obj) it works as expexted.
e.g. when I remove this line, the project is built correctly, and the specified functions located in the RAM.
What could be the problem? Should I explicitly add rts2800_ml.lib to the project? and if so, How do I remove the -ml option from the linker command?
Thanks, Isak.