Hey guys; does anyone know our planned release support for OMAP5432 support? I saw that the OMAP5432 is JTAGable in CCS 5.4; but there are still no configs, or even the notion of selecting an A15 as the project type in CCS. I've been telling my customers to just use a Generic A8 device type; and I guess a 5430 as the target in the ccxml file for JTAG? Wondering when we get an actual OMAP5432 uEVM as the target and A15 project support; alsong with all the built in register definitions into CCS (I think you still need CSP patch to support OMAP5, yes?) (I'm actually downloading this now to try...)