Hi all,
Just purchased a EVM6657LS with supplied XDS200 emulator. I loaded the CCS v5.2.1 supplied on the DVD but it did not have support for the XDS200 emulator.
So I upgraded the installed CCS v5.2.1 to CCS v5.4 which does have support for the XDS200, however when I try to launch the configuration it says it requires a license!!!
The product spec says it comes with a free copy of CCS ???
Have I done something wrong on the install?
Does the free copy only work with built in XDS100 emulator???
Regards
Anthony