Other Parts Discussed in Thread: CCSTUDIO
- Version of the host OS: Windows 7 Enterprise, 64 bit, Service Pack 1.
- Provide exact version number of CCS: 5.4.0.0091.
- If applicable, exact device/board: XDS100 (TMSDOCK28335 experimenter's kit).
- A detailed and reproducible test case: installed from the web on a new machine that did not have Eclipse or CCS installed at all. I selected some JTAG devices that don't exist on this machine; perhaps this is part of the problem (but surely it should not abort the install.) From memory, I only unchecked the Spectrum Digital drivers. I first tried using a 5.3.0 installer that I still had in the downloads directory (netword drive); it failed the exact same as 5.4.0 did. The install was not complete, e.g. no icon. I managed to start it once by searching for ccstudio.exe under c:\ti. After the first time, I set up a shortcut to it, but that fails (The Ccstudio executable launcher was unable to locate its companion shared library). That's when I tried the latest version, now 5.4.0. I was asked to attach a zip of an install folder: 0728.60556FE5-C1A1-4061-8DF8-FFB8393BAE2D.zip [ Edit: I was not able to disable anti-virus software (managed system). The antivirus software is Sophos 10.0. I could possibly get the admins to disable if you think it would help. ]
- Diagnostic logs (if available): see above. Hope I got that right.
- If the issues are related to debug: N/A.