Other Parts Discussed in Thread: MSP430F5438A
Hallo there,
using CCS Version: 4.2.4.00033 with MSP-FET430UIF, and a MSP430F5438a i recognize a strange behavior during debugging.
When i want to watch 64-bit values, they are shown as value "0" in the watch window.
When checking the memory content, the value can be read out there, which is unequal to "0".
Is there any way to show the values correctly in the watch window?
Obviously the 8-bit values are shown correctly...
Best regards,