Other Parts Discussed in Thread: CCSTUDIO
Hello,
I received an installation error while performing an update from CCS. I was told to post the contents of a folder here:
Stephen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CCSTUDIO
Hello,
I received an installation error while performing an update from CCS. I was told to post the contents of a folder here:
Stephen
Hi Stephen,
It looks like there was a problem installing the emulation package. Could you please send me the latest log from C:\Program Files (x86)\InstallJammer Registry\Emu_Logfiles\CC4C2790-5E02-4F89-9C88-2444585A2957? The filename should be something like TI_ti_emupack_install.log*
Thanks
Danish
--------------------------------------- ------ ti_emupack Installation ------------- --------------------------------------- 06/06/2013 15:19:08PM - InstallID=7D489899-A85F-4430-AA72-002C16A24043 06/06/2013 15:19:08PM - 06/06/2013 15:19:08PM - Checking conditions for 7537A6D4-E2F2-4A11-AE80-969909C92BD0 - - Before Action is Executed 06/06/2013 15:19:08PM - Checking condition C4447858-1116-47CB-95F0-BD317F6248D2 - String Equal Condition 06/06/2013 15:19:08PM - Checking to see if <%Update%> equals 1 06/06/2013 15:19:08PM - ** Checking to see if 0 equals 1 06/06/2013 15:19:08PM - Condition failed 06/06/2013 15:19:08PM - Skipping action 7537A6D4-E2F2-4A11-AE80-969909C92BD0 - Write files to the tmp file - conditions failed 06/06/2013 15:19:08PM - Checking conditions for A0103DB0-BD63-4787-A2EB-363476A78BF8 - - Before Action is Executed 06/06/2013 15:19:08PM - Checking condition 80F2FA11-D92C-4456-8EAC-0BD406E5BE49 - String Equal Condition 06/06/2013 15:19:08PM - Checking to see if <%Update%> equals 1 06/06/2013 15:19:08PM - ** Checking to see if 0 equals 1 06/06/2013 15:19:08PM - Condition failed 06/06/2013 15:19:08PM - Skipping action A0103DB0-BD63-4787-A2EB-363476A78BF8 - Update Begin Record - conditions failed 06/06/2013 15:19:08PM - Executing action 2705D3C0-E354-43BF-B8B3-031A944B936B - Set components inactive 06/06/2013 15:19:08PM - Executing action 32B0C9B9-5B56-4BEC-BD9A-596FCFE0021F - Install Selected Files 06/06/2013 15:19:08PM - Skipping component 93CC1F8F-2DDC-4939-B214-955E439B1277 - C5400 - component is inactive 06/06/2013 15:19:08PM - Skipping component 71CAEC3F-F9A7-4A00-AB57-34E29687365B - C5500 - component is inactive 06/06/2013 15:19:08PM - Skipping component 106BD0BF-4D68-4B7A-9F77-64DFBF72B6DC - C6000 - component is inactive 06/06/2013 15:19:08PM - Skipping component 8C5F906B-38FF-47C6-BDC4-A75BD3FC9C26 - OMAP - component is inactive 06/06/2013 15:19:08PM - Skipping component E5BC012C-C145-4DC9-B62C-65CAA9A6BA44 - DaVinci - component is inactive 06/06/2013 15:19:08PM - Skipping component 24731CB9-85BA-4ED8-B90F-299593B63E44 - XDS560 - component is inactive
We can try re-running that installer. Can you check to see if you have the file ti_emupack_setup_5.1.114.0.exe or ti_emupack_setup_5.1.114.0.exe.bk in the eclipse/downloads folder? If so, can you run it with the following parameters on a cmd prompt started in the downloads folder?
ti_emupack_setup_5.1.114.0.exe /noc2400 /noc5400 /noc5500 /noc6000 /noomap /nodavinci --prefix "C:/ti/ccsv5/ccs_base" /noxds560
If the file doesn't exist in the downloads folder, you can download it from here: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/emulation/exports/ti_emupack_setup_5.1.114.0.exe
Let me know if you run into any issues.
Danish
Stephen,
Do you mean the start up menu and desktop shortcuts haven't been updated? That would be because the update failed to complete successfully.
Danish