This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot add some files



I am trying to add some files to my project.  I have been able to add many files successfully, but there are a couple of files that when I try to add (either through add files.... copy file or add files.... link to files) I get a message box pop up that says it could not add the files.  I have been able to add many files in this way (I would prefer to link to them).

 

Any suggestions?

 

Thanks

  • Hi David,

    could you please expand on the error you see?  Is there something unique to the files giving you problems?  (ie could it be related to permissions in a certain directory, are you using version control and trying to pull in a checked out file, etc) 

    Perhaps some screen captures and or a sample file for us to try might help.

    Best Regards,
    Lisa

  • As far as I can tell there is nothing special about the files.  They exist in the same directory and came from the same place in the same way that files I was able to add are. None of the files have been checked out of source control.

    Below is a picture of the error I am seeing.  I will try sending an example file to you privately.

     

    Thanks,

    David

  • Hi David,

    thanks again for the update and time offline.  Glad to hear it was duplicate naming.

    All the best with development.

    Best REgards,
    Lisa