Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi there,
When I have changed the OMAP-L138 Experimenter Kit onto our own development board with LogicPD SOM with OMAP-L138 (the same as on Experimenter Kit) and use XDS100v2 from Spectrum Digital I have following problem with emulating the same project as before:
ARM9_0: Output: Target Connected.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Cleared.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: KICK Unlocked.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PSC Enable Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PLL0 init done for Core:300MHz, EMIFA:25MHz
ARM9_0: Output: mDDR initialization is in progress....
ARM9_0: Output: PLL1 init done for DDR:150MHz
ARM9_0: GEL: Error while executing OnTargetConnect(): Attempted to write unmapped virtual memory at 0xB00000E4.
ARM9_0: Trouble Writing Memory Block at 0xc392373c on Page 0 of Length 0x7ff0: (Error -2030 @ 0x72637365) Internal error: Access to unknown or invalid register was requested. Restart the application. If error persists, please report the error. (Emulation package 5.0.520.0)
ARM9_0: GEL: File: C:\U...\build\Debug\UPPDriver.out: Load failed.
ARM9_0: Unable to terminate memory download: NULL buffer pointer at 0x320
I need to turn off and on the board to make it run and it runs only once. Each time I want to emulate second time after powering it up it show me this message. Any idea where to look for solution?