Other Parts Discussed in Thread: UCD3138
Hi All
I am using UCD3138 for an LLC resonant converter, and am working with CCS 5.4. I got the following erros and have no idea how to fix it. If you know, please help me to fix these errors:
**** Build of configuration Debug for project UCD3138LLCEVM_028 ****
"C:\\codecomposer5.3\\ccsv5\\utils\\bin\\gmake" -k all
(rm device_id.obj) & (perl ../../build_scripts/create_date_dot_h_CCS5.pl)
'rm' is not recognized as an internal or external command,
operable program or batch file.
'perl' is not recognized as an internal or external command,
operable program or batch file.
gmake[1]: [pre-build] Error 1 (ignored)
' '
'Building target: UCD3138LLCEVM_028.out'
'Invoking: ARM Linker'
"C:/codecomposer5.3/ccsv5/tools/compiler/arm_5.0.5/bin/armcl" -mv4 --code_state=16 --abi=tiabi -O1 -g --preproc_with_compile --preproc_with_comment --diag_warning=225 --display_error_number -z --stack_size=200 -m"C:/test1/CCSv5-untested/UCD3138LLCEVM_028/UCD3138LLCEVM_028.map" --heap_size=10 -i"C:/codecomposer5.3/ccsv5/tools/compiler/arm_5.0.5/lib" -i"C:/codecomposer5.3/ccsv5/tools/compiler/arm_5.0.5/include" --reread_libs --warn_sections --display_error_number --rom_model -o "UCD3138LLCEVM_028.out" "./zero_out_integrity_word.obj" "./uart.obj" "./store_restore_functions.obj" "./standard_interrupt.obj" "./software_interrupt_wrapper.obj" "./scale.obj" "./pmbus_vout_sequencing_commands.obj" "./pmbus_vout_commands.obj" "./pmbus_status_commands.obj" "./pmbus_read_param_commands.obj" "./pmbus_other_commands.obj" "./pmbus_manuf_specific_commands.obj" "./pmbus_manuf_info_commands.obj" "./pmbus_handler.obj" "./pmbus_fault_commands.obj" "./pmbus_cml_commands.obj" "./pmbus.obj" "./main.obj" "./load.obj" "./interrupts.obj" "./init_watchdog.obj" "./init_pmbus.obj" "./init_loop_mux.obj" "./init_front_ends.obj" "./init_filters.obj" "./init_fault_mux.obj" "./init_dpwms.obj" "./init_current_sharing.obj" "./init_cpcc.obj" "./init_adc12.obj" "./gpio.obj" "./flash.obj" "./device_id.obj" "./cyclone_global_variables_defs.obj" "./constants.obj" "./configuration_functions.obj" "./clear_program_flash.obj" -l"C:\codecomposer5.3\ccsv5\tools\compiler\arm_5.0.5\lib\libc.a" "../cyclone.cmd" "../cyclone_headers.cmd"
<Linking>
undefined first referenced
>> Compilation failure
symbol in file
--------- ----------------
$c_int00 ./load.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "UCD3138LLCEVM_028.out" not
built
gmake[1]: *** [UCD3138LLCEVM_028.out] Error 1
gmake[1]: Target `main-build' not remade because of errors.
gmake: *** [all] Error 2
**** Build Finished ****
Thanks,
Mehran