This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS still holds focus when minimised

CCS 5.4.0.00091 win 8 & win 7 (and with previous v5 releases on same OS's)

A small issue, if I minimise the code composer studio window, either with the minimise window control or with alt -> space -> n key sequence, the window still holds focus instead of it being handed back to whatever other application is then available next on the desktop.

This does not appear to happen with any other applications on the two laptops I use CCS on.

Use case: Open some other application, e.g. MS word, then open or move to already open CCS window, leaving the MS word window on the desktop but with CCS "in front of it". Then minimise CCS so MS word is visible, then use a keyboard shortcut for something that should work in MS word as focus should now be with Word, e.g. alt+f4, the result SHOULD be that  MS Word closes - INSTEAD CCS does.

Small problem - VERY annoying!