Looks like #pragma message is not supported in TMS470?
Also I couldnt get exact syntax for #warning?
Can you give the exact syntax. I am using ccs 5.0.4
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Looks like #pragma message is not supported in TMS470?
Also I couldnt get exact syntax for #warning?
Can you give the exact syntax. I am using ccs 5.0.4
This is a feature of most C compilers which is not specified in the C89 or C99 standards. In the TI compiler it is ...
#warn your message here
Thanks and regards,
-George
to implement deprecated warming i have something like,
/* Deprecated function - Compiler message */
#ifdef __GNUC__
#define DEPRECATED(func) func __attribute__ ((deprecated))
#elif defined (__TMS470__)
#define DEPRECATED(func) func
#warn Some of the DEPRECATED functions are used, please use migrate to supported functions
#elif defined (__IAR_SYSTEMS_ICC__)
#define DEPRECATED(func) func
#pragma message("WARNING: You need to implement DEPRECATED for this compiler")
#else
#error unsupported compiler!!!
#endif
For CCS, it gives the line number where #warn is defined and i want the line number of the deprecated function.
Do you have better suggestion for this issue.
Thanks
Baskaran
The TI compilers support many GCC extensions, including the deprecated function attribute. You have to build with the switch --gcc. Please see this wiki page for the details.
Thanks and regards,
-George