This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connection for OMAPL137 is missing

Hi,

I am running the CCStudiov5.4 on Linux 2.6.

In target configuration, there is no board type available under "Spectrum Digital DSK-EVM PLUS onboard USB Emulator". I try to add the board myself by selecting the "EVMOMAPL137" from board, "OMAPL137" from Devices and "ARM9" from CPU library.

But it shows an error:

"Unable to find an appropriate device driver for the connection type "SD510DSK" and isa "ICEPICK_C". Please choose a different component"

I though it may miss some files when installing. So I reinstalled it but it didn't help.

I am now using a free version. Is the free version prevent me to use this connect?

Thank you!

Zhe