This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5 installations issues



am trying to download CCSv5 and I keep running into the following error message:

 

Unable to access http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/CCSv5/CCS5.4.0.00091_win32. Check your settings and try again.

 

The ref_url: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/CCSv5/CCS_5_4_0/  does not exist. Clicking on it gives me the "File not found" page.

I looked this up online and the recommendation was to try the full installer. I have also tried the full installer and  it get stuck at Jre extraction.

 

I am kind of stuck and need urgent help to install this.

I had spent full day to figure out a way to get out it.

It should have have automatic dependency check to help user.

Installation should be easy .

but somehow looks like CCS 5 is not doing that.

here is post which i posted may be in wrong place to get clean installtion done correctly.

----------------------------------------------------------------------------------------------

http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/273821/956201.aspx#956201

  • I'm sorry you're having problems with your installation. Could you zip up the contents of the folder c:\program files\installjammer registry\ccsv5 (program files (x86) if you're using a 64 bit machine) and post them here? Please note, installjammer registry is a hidden folder.

    I'll get back to you as soon as I've taken a look at the logs.

    thanks

    Danish

  • I was able to fix it.Link has the issue and way to get out of it.

    But looks like this issue is there from long time but no one taken care to resolve.

    Link also has log in one of the last post before fix.

    http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/273821/956201.aspx#956201