Other Parts Discussed in Thread: SYSBIOS
I have this huge shared code base which spans bios 4.9 up to bios 6.34.4.22. I cannot upgrade the current stuff to 6.35 due to the final killing off of xdc.runtime.LoggerBuf.
This stuff goes back years and I am not too sure how to rearrange things and not kill off stuff from long ago, so in the code base it still needs to call "LOG_printf(&ces_log,...", but only need to know what to use instead for the current project to achieve something similar with UIA.
The cfg file has this:
if (useDebugBIOS)
{
var Agent = xdc.useModule('ti.sysbios.rta.Agent');
xdc.print("Building with DEBUG bios.\n");
}
else
{
xdc.print("Building with RELEASE bios.\n");
/* .. and an old-style LOG_Printf() is at level INFO */
Main.common$.diags_INFO = Diags.ALWAYS_ON;
}
...
var log_params = new LoggerBuf.Params();
log_params.bufSection = "SDRAM";
log_params.numEntries = 256;
var ces_log = LoggerBuf.create(log_params);
if (!useDebugBIOS)
{
Main.common$.logger = ces_log;
}
/* An old-style LOG is secretly a LoggerBuf */
Program.symbol["ces_log"]=ces_log;
...
if (useDebugBIOS)
{
BIOS.logsEnabled = true;
Agent.sysbiosSwiLogging = true;
Agent.sysbiosHwiLogging = true;
Agent.sysbiosTaskLogging = true;
Agent.sysbiosLoggerBufferSection = "offchip_text";
Agent.sysbiosLoggerSize = 65536;
Agent.loadLogging = true;
Agent.loadLoggerBufferSection = "offchip_text";
Agent.loadLoggerSize = 8192;
Agent.mainLoggerBufferSection = "offchip_text";
Agent.mainLoggerSize = 32768;
Agent.mainLogging = true;
}
Logging ends up at "Void LOG_printf4(LOG_Handle handle, String format, ...)", where should I arrange for it to end up at now?
Chris