Hi There,
I've just tried to install the latest code-composer version (ccs_setup_5.4.0.00091), never having used the tool before. When running the setup-file, it just crashes, with no dialog or pop-up indicating what the problem is. I've found the following error text in the Windows event log:
Faulting application name: ccs_setup_5.4.0.00091.exe, version: 5.4.0.91, time stamp: 0x4fe2322a
Faulting module name: ccs_setup_5.4.0.00091.exe, version: 5.4.0.91, time stamp: 0x4fe2322a
Exception code: 0xc00000fd
Fault offset: 0x000223e7
Faulting process id: 0x1738
Faulting application start time: 0x01ce71238d75729d
Faulting application path: C:\Users\Dave\Downloads\ccs_setup_5.4.0.00091.exe
Faulting module path: C:\Users\Dave\Downloads\ccs_setup_5.4.0.00091.exe
Report Id: cc902172-dd16-11e2-be74-bcaec5021af2
Machine details are:
ASUS EB1501P Nettop.
Intel Atom D525 CPU @1.8GHz
2GB RAM
Windows 7 Home Premium (64-bit)
NVidia ION Graphics - driver version 3.20.18
I do wonder if it's related to the NVidia issue mentioned here. However, I don't have an Optimus chipset - and the NVidia control panel doesn't have the "Preferred Graphics Processor" option mentioned in that solution.
Can anyone help?
Cheers,
Dave