This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error initializing emulator,unenable connect to target.



 Hi.

 When I open CCS and try debug,it give me the message:

"(Error initializing emulator )

 Unable to communicate with the emulator.

  confirm emulator configuration and connections,reset the emulator,and retry the operation."

  I use windows 7,CCS version is 5.2.1.0018.

  When I use windows xp ,with the same configure,it works well.