We are doing some research about LTE communications by using the Neocific Mamba board. The processor on the board is TMS320C6457. We also use the Spectrum Digital XDS510USB Emulator with a JTAG low voltage adapter to convert the voltage from 3.3V to 1.8V. We use CCS 5.3.
The program has been compiled successfully. But when we open the debugger and try to download the .out file to the target board, it says “Error connecting to the target: Connect to PRSC failed, -6305”.
We really don’t know what’s going on. Please give us some suggestions.
Thanks!