Hi Lisa and all,
I am having difficulties getting CCS v5.4 installed too. I was directed to use off-line installer, but in vain. Please see the attached file. 1854.ccs_setup_5.4.0.00091_install.log
Thanks,
Sean
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lisa and all,
I am having difficulties getting CCS v5.4 installed too. I was directed to use off-line installer, but in vain. Please see the attached file. 1854.ccs_setup_5.4.0.00091_install.log
Thanks,
Sean
Hi Sean,
do you have an NVIDIA graphics card? From the log, it seems like you might be hitting a known incompatibility with them.
One work around is posted here:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/262977.aspx
Best Regards,
Lisa
Thanks, Lisa.
I managed to install it successfully when running Win 7 under the safe mode. However, I cannot activate the installed CCS v5.4. CCS is not responding after I select a workspace. Would you please shed some on light on this issue?
Best regards,
Sean
Hi Sean,
glad to hear you seem a step further. Does this also happen if you create a new workspace?
Could you have a look at this wiki and send any dump files or error logs?
http://processors.wiki.ti.com/index.php/Troubleshooting_CCS
Best Regards,
Lisa
I really appreciate your prompt reply, Lisa. It helps me move ahead greatly.
You were right that it went through with a new workspace. Does it mean that I cannot open an existing workspace which was prepared with v4? Should I import it again to v5.4?
Thanks,
Sean