This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestion for Improvement: Multiple MSP-FET430UIF Tools

I'm currently working on a project which requires two MSP430 devices in different hardware configurations to communication.  To facilitate development I run two instances of CCS5.4 pointed at different workspaces for each MSP.  However, each one must use a specific FET that is connected to my workstation.

Currently in the Target Configuration editor, it lists: TI MSP430 USB1, USB2, and USB3.  These three entries are rather arbitrary, and do not seem to relate to a specific FET tool.  This becomes problematic in environments like mine where each workspace needs to connect to a specific MSP.

It would be far more useful in instances like these to allow the selection of a specific FET COM port.  Each FET tool enumerates in the device manager with a COM port, which I can relate to the specific piece of hardware by watching the enumeration sequence as the debuggers are connected to the USB port.  There can still be a default or automatic selection option, but with the addition to choose a specific one.

Thanks for the consideration,

Bart Basile