This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with the linker



Hi!

I have a eZdsp C5515 USB Stick and i'm trying to get interrupts from Timer0. Well, for this purpose i created new CCS project and tryed to build it.
But i got linking problems like this:

 ------------------------------------------------------------------------------------------------------------------------------------------------------

<Linking>

undefined  first referenced                                                                                        

  symbol       in file                                                                                                     

_main     C:\\Program Files (x86)\\Texas Instruments\\ccsv4\\tools\\compiler\\c5500\\lib\\rts55x.lib<args_main.obj>


error: unresolved symbols remain

error: errors encountered during linking; "Timer_INT.out" not built

--------------------------------------------------------------------------------------------------------------------------------------------------------

So, i have  project with: vector.asm fiile, the linker cmd file, source file, all nessesary include files.

This is full project in zip-file:0167.Timer_INT.zip

And this is my building properties with library search path section:

It seems the problem in rts55x.lib.

How can i fix this problem?

Regards,

Nick